NEW Raspberry Pi Camera Module - Order Today
5mp and 1080p full HD video recording

Raspberry Pi

Place your order today.

The Raspberry Pi is a credit-card sized computer board that plugs into a TV and a keyboard. It’s a miniature ARM-based PC which can be used for many of the things that a desktop PC does, like spreadsheets, word-processing and games. It also plays High-Definition video. The Raspberry Pi Model A and Model B boards are supplied as board only, and come without operating system, SD card, power supply, keyboard, case or cables.

You are now able to purchase as many Raspberry Pi board's as you require. Simply select from the two options below to start your journey. Please note you will be advised of an expected lead times at point of order.

Personal use
Business use
Raspberry Pi Limited Edition Boards

Raspberry Pi Limited Edition Boards

To celebrate the first anniversary of Raspberry Pi, we're giving away 1,000 limited edition blue Raspberry Pi Model B boards complete with blue user case and certificate of authenticity. Find out more about our special anniversary Pi's and how they'll be donated to good causes here.

Raspberry Pi

Features of the Raspberry Pi Boards (Model A and Model B)

  • Broadcom BCM2835 700MHz ARM1176JZFS processor with FPU and Videocore 4 GPU
  • GPU provides Open GL ES 2.0, hardware-accelerated OpenVG, and 1080p30 H.264 high-profile decode
  • GPU is capable of 1Gpixel/s, 1.5Gtexel/s or 24GFLOPs with texture filtering and DMA infrastructure
  • 256MB RAM (Model A), 512MB RAM (Model B)
  • Boots from SD card, running a version of Linux
  • USB 2.0 socket (Model A x 1 socket/ Model B x 2 sockets)
  • 10/100 BaseT Ethernet socket (Model B only)

Raspberry Pi frequently asked questions

Why won't my Raspberry Pi boot up?

If your 512MB Raspberry Pi has a Hynix memory chip in the middle of the board (that’s the black, square RAM chip right in the centre, and it’ll either say Samsung or Hynix on it in white letters), please ensure you are using the latest version of Raspbian which you can download by clicking here.The version on this link will always be the latest available.

© RS Components Pty Ltd ABN 73 009 403 356, 25 Pavesi St, Smithfield. NSW. 2164 (PO Box 6864, Wetherill Park. NSW. 1851)
Orderlines: 1300 656 636 (8.00am-7.30pm AEST Monday-Friday)/ RS Web Helpline: 02 9681 8500 (8.00am-6.30pm AEST Monday-Friday) OR email: oztech@rs-components.com